General Settings

Use this dialog to select the desired language for the software user interface and Help and also configure your proxy settings if necessary.

Language Selection

From the main Global Settings menu, you can select the desired language for the BenchVue software user interface and Help. Select the desired language from the drop-down list and click "OK" to show the user interface, dialog boxes, status messages, and Help in the selected language.

Proxy Settings

Select "Use Proxy Server" to configure a proxy server. A proxy server is a computer that acts as a gateway between a local network and a larger-scale network such as the Internet. Proxy servers are often used to provide increased performance and security. To configure the desired proxy server, specify the IP address (host) and port number of the proxy server. Click "Validate" to confirm the IP address and port number.